Launch IO Control

With IO Libraries 2026, IO Control is available as a utility. You can launch it the following way:

From the taskbar notification/tray area:

In Windows, IO Control is installed in the notification / tray area of the taskbar. It provides quick access to many utilities and help files. Depending on system configuration, this is typically on the bottom right of the screen, near the system clock. The IO Control icon may appear directly on the taskbar, or it may be nested with hidden icons.

With IO Control, you can launch applications and utilities, and open help documentation included in Keysight IO Libraries Suite. Applications include:

Application and Utilities IO Libraries Help Docs
  • Connection Expert
  • IO Monitor
  • Interactive IO
  • New Connection Expert
  • New IO Monitor
  • New Interactive IO
  • Event Viewer
  • ViFind32 (debug utility)
  • ViFind64 (debug utility)
  • Add Legacy PXI Chassis
  • Direct Connect
  • Set 32-Bit Primary Visa
  • IO Libraries Suite Help
  • VISA Help
  • VISA.NET Help
  • VISA COM Help
  • SICL Help
  • Keysight 488 Help
  • Keysight Connectivity Online
  • Secure Instrument Communication Expert Setup Guide
  • IO Libraries Readme